Solid Edge Balloon Command Default settings

Experimenter
Experimenter

Hello,

 

Is it possible to connect to Solid Edge while in a draft document and change the "default" settings on the Balloon command bar? For instance, If I have a draft and click the balloon command it will have the previous settings preselected from the last balloon placed. I want to be able to change between different balloon shapes, heights, ect. without me having to do it manually all the time.

 

I tried connecting to SolidEdgeFramework.CommandBar but I'm not sure if that's the right approach. I typically code in C# but I can translate VB stuff is somebody can come up with anything.

 

Thanks for any help!

1 REPLY

Re: Solid Edge Balloon Command Default settings

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi,
The only way to manually select a saved setting.
I think there is no way to change this via the API while Solid Edge
is running.
regards

JB
SE ST10