Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Customization

Valued Contributor
Valued Contributor

All,

 

I need to assemble components in an assembly using coordinate system by providing X,Y,Z dimensions from the default coordinate system with the help of customization. Can anyone help me how to achieve that with Coding?

Also, is it possible to create dimensions in draft files by using customization. If yes, how can we do that?

 

Best regards,

Thiyagarajan.

 

Posted by: thiyagarajan d
Post date: 3/2/2012 8:53:58 AM

1 REPLY

Re: Solid Edge Customization

Valued Contributor
Valued Contributor

Yes! It is possible, but for that you need to find out the relations between parts and then you need to align the parts. But I suggest if you could make a parametric model then it is very easy to program. You can hide or delete the parts which you don’t require and this way you can manage the assembly and their parts.

 

If your requirement is different than in solid Edge help you will find some example like how to use Geometric Constraints, by using those example you need to find the surface, edge or axis of part as well base part and provide the respective constrain.

 

Sandeep Shewale

 

Posted by: Sandeep Shewale
Post date: 4/2/2012 6:36:55 AM