Cancel
Showing results for 
Search instead for 
Did you mean: 

Solid Edge Synchronous : Sheet Metal Edit problem

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Dear All,

 

I am working with a client on sheet metal synchronous technology, their we are facing some issue like

i have created a base flange followed with tab flange. On my side flange i have created a cut of 125 degree on 100 mm from top and then created a contour flange followed by few operations like hole, dimple cut out. Now if want to edit that 125 degree to 110 degree, i am not able to do that without deleting it

Sheet metal file is also attached. Please help me in this regards. 

 

Regards,

Saksham Hans

1 REPLY

Re: Solid Edge Synchronous : Sheet Metal Edit problem

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Please ask your question in the Solid Edge Forum of the Solid Edge User Community, as this is a developer forum, which addresses SE customization via API.

You will get better feedback in the other forum.