Solid Edge as an Ole Object in Crystal Report

Valued Contributor
Valued Contributor

I have an integrated Crystal Report that i need to insert a Solid Edge object. Using Ole Objects, and inserting a Solid Edge .dft document works fine. The issue comes in when i need a dynamic link that inserts the xxx.dft that is linked to an item path that is stored in Sequel at run time. Any ideas or help would be appreciated. (btw, am also using the PowerToys for Solid Edge, works great!) Thanks

 

Posted by: Jennece Wilson
Post date: 2/16/2012 9:31:49 AM

1 REPLY

Re: Solid Edge as an Ole Object in Crystal Report

Valued Contributor
Valued Contributor

Jennece,

 

I must admit to having zero experience with Crystal Reports. I would expect (assume) that there is an API for Crystal Reports that you could use to emulate the functionality that you describe. Regarding OLE Objects, SQL server and such, I could assist with if you need. Perhaps there is a Cyrstal Reports user group somewhere that can help?

 

Glad PowerToys is working for you ;-)

 

Posted by: Jason Newell
Post date: 2/21/2012 5:07:58 PM