Cancel
Showing results for 
Search instead for 
Did you mean: 

Solidedge BOM

Valued Contributor
Valued Contributor

Hi this is Ravi,

 

I have Solidedge ST2 version,

In Program files there is a folder named custom in SE folder, which has  lot of application.

BOM is one of them. If I run the BOM.exe, I get the required result that it is giving the BOM structure same as Assembly structure in SE.

but there is one detail is missing for me and that is Material, there is no materia tab.

 

can any one give me modified BOM.exe so that I can get my required BOM structure.

 

please reply soon..

thanks in advance.

 

 

Posted by: Ravindra Borhade
Post date: 12/22/2010 11:37:28 PM

2 REPLIES 2

RE: Solidedge BOM

Valued Contributor
Valued Contributor

Hi Ravi

 

I haven't been around here for a while and saw you r topic today.

here is a quick revision of BOM. I changed the "creation date" option (which i never used) into "material".

I'm using V20 but i think it should work on ST2 as well. I hope its not too late for you and can serve you.

VH

Alon

 

p.s

it seems imposible to upload an *.exe file. so once you have bom_material change its name and add ".exe"to the and to make it work..

 

Posted by: alon raviv
Post date: 1/19/2011 4:38:34 AM

RE: Solidedge BOM

Valued Contributor
Valued Contributor

Posted By ara on 19 Jan 2011 10:38 AM

it seems imposible to upload an *.exe file. so once you have bom_material change its name and add ".exe"to the and to make it work..

The forums are configured for .zip attachments and are preferred.  Thanks.

 

 

Posted by: Jason Newell
Post date: 1/19/2011 5:30:44 AM