Cancel
Showing results for 
Search instead for 
Did you mean: 

TC - Solid Edge Session

Valued Contributor
Valued Contributor

Hi ,

 

I have a requirement where I need to launch a Solid Edge assembly from Teamcenter 8.3.

 

The complete assembly is present on Tc 8.3, I need to load the assembly into Solid Edge(Just like NXManager).

 

I have done only SE customization only based on local files...

 

I have a small idea that it can be done using Revision Manager.dll

 

Please help....

 

Posted by: Jacob Andrews
Post date: 5/7/2013 1:01:13 AM

1 REPLY

TC - Solid Edge Session

Valued Contributor
Valued Contributor

'objapp is the object of the Solid edge session

Dim setc As SolidEdgeFramework.SolidEdgeTCE = objApp.SolidEdgeTCE

Dim strUserName As String = <string>

Dim strPassword As String = <string>

Dim strGroup As String =<string>

Dim strRole As String = <string>

Dim strURL As String = "https://tcserver/webclient"

Dim stritem As String = <string>

Dim strrev As String = <string>

Dim dft As String = <string>

Dim rule As String = <string>

Dim fol As String = "D:\output"

setc.ValidateLogin(strUserName,strPassword,strGroup,strRole,strURL)

 

 

I tried it in the TC environment command prompt .....

 

// the validate login api is throwing COM error while debugging...

 

 

Is it possible that this error is coming due to the license not enabled for vb.net apis to integrate with Teamcenter....

 

any other reasons ???

 

Posted by: Jacob Andrews
Post date: 5/8/2013 11:42:00 PM