Reply

TSEpartX - error when open par or asm

[ Edited ]

 

Hello,

 

I would like to use TSEpartX (3D viewer) component in my apllication, I put this component  on a form and I run it.

When I try to open par or asm I get error "Floating point division by zero". The error is probably caused by Markup3D.dll or Jt61.dll.

TSEDraftX1 (2D viewer) works without any problems.

I use Delphi and Solid Edge Viewer 20.

I have registered in Winows all ocx controls which I found in Solid Edge Viewer directory.

regsvr32 SEDraftX.ocx

regsvr32 SEListCtrlX.ocx

regsvr32 SEpartX.ocx

regsvr32 SEPropVwX.ocx

regsvr32 SEStructVwX.ocx

and all dll's which are used in Markup3D.dll or Jt61.dll.

I still have got this error.

I noticed that nobody uses Delphi + SE, but what's about VB ? Has anybody tried to use this viewer ? Any idea how to avoid this error ?

kind regards

ZS

 

Posted by: Zbigniew Sorokowski
Post date: 10/7/2008 2:29:26 AM

1 REPLY

RE: TSEpartX - error when open par or asm

[ Edited ]

 

I installed VB 2008 and I see that SE ActiveX works in VB without any problems.

It means that the Delphi is a source of problem, not SE.

I let you know if I solve this problem.

kind regards

ZS

 

Posted by: Zbigniew Sorokowski
Post date: 10/8/2008 12:44:53 AM