Cancel
Showing results for 
Search instead for 
Did you mean: 

Trace curve feature in Solid Edge ST6

Experimenter
Experimenter

Hello!

 

I want to know if Solid Edge ST6 has the tool "Trace curve," like Pro/ENGINEER has, beacuse I have to send a project to a teacher of mine and he told me to use this feature. The mechanism I created is the Artobolevsk's mechanism to trace the Diocle's curve (as you can see here, if you have Wolfram CDF Player plugin installed in your computer) and I have to demonstrate the curve while the system is running. I created the whole project using Solid Edge ST6 due to its simple interface.

 

If, for some reason, SE ST6 doesn't have this feature, I was thinking about changing the files format, in order to open them with ProE. Do you have any objection to this idea? Do you think it will work?

 

@Edit: I see now it's not the right place to post my question. I'll do it in the right forum!

 

Thank you for any help you can provide,

Leonardo Monteiro de Carvalho

1 REPLY

Re: Trace curve feature in Solid Edge ST6

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Leo,

 

I am not able to see the mechanism since the CDF player is not installed on my machine.

Its a whopping 200 MB download Smiley Surprised

 

Perhaps you can record the screen and share on screencast.com.

I read the ProE online help about tracing and understood the functionality.

 

But you have by mistake posted this Q in the correct forum.

With little help using programming, a point in the mechanism can be traced.

I can see, I can do this using a .Net program.

 

 

Well, that would be quite some effort.

Let me know if you are interested.

 

~Tushar Suradkar

http://surfandcode.blogspot.in/