Cancel
Showing results for 
Search instead for 
Did you mean: 

Unique ID For Objects

Valued Contributor
Valued Contributor

 

I come from AutoCAD background.

 

When you create an object (even non-graphical object like blockdefinition) in AutoCAD, AutoCAD assigns a unique (in that

 

drawing) ID to it. (As far as I remember, only selection sets do not have handles). AutoCAD retains this handle even when

 

that object is deleted. It is not assigned to any other object in that drawing.

 

In programming, this handle is available as EntityName in AutoLISP and ObjectID in VB. (These are however different from the

 

handle). This has many advantages, especially in programming.

 

For example, I can share the same object in multiple languages using conversion like EntityName > Handle > ObjecttID and vice

 

versa. Also storing objects in variables becomes easier.

 

Most of the Solid Modellers (Inventor, SolidEdge) must be having this concept internally. However, none of them expose

 

anything similar to handle in API. This causes inconvenience in identifying objects and storing them in variables.

 

They provide other facilities like ReferenceKey or Attributes. But this means extra work for the programmers.

 

My questions:

 

1) Why solid Modelling APIs do not provide this facility. What could be the pros and cons.

2) Do you think they should provide this for making the life of Progrmmers a bit more easier?

 

Your take on this.

- Sanjay Kulkarni 

 

Posted by: Sanjay Kulkarni
Post date: 5/29/2010 7:34:55 AM

1 REPLY

RE: Unique ID For Objects

Valued Contributor
Valued Contributor

[Copy pasted from my LinkedIn response]

 

In COM programming, each COM object has a unique pointer. You can easily compare two objects for equality using this pointer. Depending on the programming language you're using, the process of comparing may vary. I fail to see the issue.

 

Posted by: Jason Newell
Post date: 6/1/2010 7:50:11 AM