Cancel
Showing results for 
Search instead for 
Did you mean: 

UnitOfMeasure bug?

Valued Contributor
Valued Contributor

I'm trying to set the unit density of the active document (.par/.psm).

 

for the length unit, this works flawless:

        Dim app As Object, objDoc As Object
        app = GetObject(, "solidedge.application")
        objDoc = app.ActiveDocument


        objDoc.UnitsOfMeasure.Item(UnitTypeConstants.igUnitDistance).Units = SolidEdgeConstants.UnitOfMeasureLengthReadoutConstants.seLengthCentimeter

but for density the same code doesn't:

        Dim app As Object, objDoc As Object
        app = GetObject(, "solidedge.application")
        objDoc = app.ActiveDocument

        objDoc.UnitsOfMeasure.Item(UnitTypeConstants.igUnitDensity).Units = SolidEdgeConstants.UnitOfMeasureDensityReadoutConstants.seDensityGramPerMeterCubed

i've tested in ST7 and ST8

Maarten Elings | Engineer
2 REPLIES

Re: UnitOfMeasure bug?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

It's not a bug, if you consider that you CANNOT use the unit type as an index to the collection. If you want to look for a specific UnitOfMeasure object, you will need to iterate through all of them and check for the correct type.

You can verify this by simply running the following code, which shows differences between the index and the unit type for all units, except igUnitDistance and igUnitAngle!!

Dim i As Integer = 1
For Each objUOM In objDoc.UnitsOfMeasure
  Diagnostics.Debug.WriteLine("UOM(" & i.ToString() & ") = " & objUOM.Type.ToString() & " (" & CInt(objUOM.Type).ToString() & ")")
  i += 1
Next

 

Re: UnitOfMeasure bug?

Valued Contributor
Valued Contributor

Thank you!

 

Using the Constants Enumetions from the help file I obtained the right value for density so:

 

        Dim Objapp As Object, objDoc As Object
        Objapp = GetObject(, "solidedge.application")
        objDoc = Objapp.ActiveDocument

        objDoc.UnitsOfMeasure.Item(6).Units = 4 'sets the Density(6) to kg/m³ (4)
Maarten Elings | Engineer