Cancel
Showing results for 
Search instead for 
Did you mean: 

Update draft views

Valued Contributor
Valued Contributor

Hello everybody,

 

Is thear a code to update a dft?

 

Regards,

 

Mariano

 

Posted by: Mariano Spini
Post date: 10/11/2010 1:27:22 PM

6 REPLIES 6

RE: Update draft views

Valued Contributor
Valued Contributor

Assuming the ActiveDocument is a Draft:

 

Application -> ActiveDocument -> ActiveSheet ->DrawingViews(n) -> Update

 

You can use DraftDocument -> Sections -> WorkingSection if you need to only look at WorkingSections.

 

Posted by: Jason Newell
Post date: 10/11/2010 1:40:08 PM

RE: Update draft views

Valued Contributor
Valued Contributor

Ok, but is there any code to update all the draft file?

Samething like startcommand or similar that execute the same function as the icon?

I also need to fit the view.

 

Regards,

Mariano

 

Posted by: Mariano Spini
Post date: 10/11/2010 1:58:30 PM

RE: Update draft views

Valued Contributor
Valued Contributor

I'm not sure if it's exactly the same with Draft but this is what I use with models.

 

Dim oApp As SolidEdgeFramework.Application

Dim oDoc As SolidEdgeAssembly.AssemblyDocument

Dim fit_window As Object

 

'Connect to the running instance of Solid Edge.

oApp = Marshal.GetActiveObject("SolidEdge.Application")

'Open the file.

oDoc = oApp.Documents.Open("file_path\file_name.asm)

 

'Update the model.

oDoc.ActivateAll()

oDoc.UpdateAll()

 

'Fit to window so you can see the whole thing.

fit_window = oApp.ActiveWindow

fit_window.View.Fit()

 

HTH

 

 

Posted by: Terry Tyson
Post date: 10/12/2010 3:34:58 AM

RE: Update draft views

Valued Contributor
Valued Contributor

It doesn't work.

 

I also try the line:

 

Call objApp.StartCommand(PartCommandConstants.PartViewISOView)

 

But it works well under windows Xp but it doen't work under windows 7.

Any idea?

 

Regards,

Mariano

 

Posted by: Mariano Spini
Post date: 10/12/2010 4:31:31 PM

RE: Update draft views

Valued Contributor
Valued Contributor

This should work. It's a small modification of the help example: Modellink.UpdateViews

HTH,

Julian

 

Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)

'Update All Drawing views associated with all ModelLinks using UpdateViews method

 

 

For each objModellink in objdoc.Modellinks

    objModelLink.UpdateViews

next

 

' USER DISPLAY

' Release objects

Set objApp = Nothing

Set objDoc = Nothing

Set objModelLink = Nothing

End Sub

 

Posted by: Julian Guillo
Post date: 10/13/2010 2:15:17 AM

RE: Update draft views

Valued Contributor
Valued Contributor

Excelent!!!! It works!

 

But I doesn't update the Bill of material (BOM).

 

Any advice?

 

And how to fit the view?

 

Thanks you in advance!!!!

Mariano

 

Posted by: Mariano Spini
Post date: 10/14/2010 5:20:05 PM