Cancel
Showing results for 
Search instead for 
Did you mean: 

Use SE Spy to get system number for selected body face

Valued Contributor
Valued Contributor

Hello All,

 

Am using SE Spy to get system number for selected body face, but can't see it. Any help?

3 REPLIES

Re: Use SE Spy to get system number for selected body face

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hello SergioH
How do you select a Face? What do you mean with "system number"?
BR
regards

JB
SE ST10

Re: Use SE Spy to get system number for selected body face

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I just saw your reply in the "Code Example for "Add Part by file name then apply..." thread.

If you select a Face item on the left side, then the properties are shown right, listing the ID and the Tag properties.

SE Spy.png

regards

JB
SE ST10

Re: Use SE Spy to get system number for selected body face

Valued Contributor
Valued Contributor
Hi, thanks for your reply. Any part model has an integer number assigned
for each face on its body. Normally when placing a part into assembly some
of these faces get selected by user to create relationships and constraint
the part. Am looking a way for knowing this integer number instead of
guessing to develop my code and constraint parts using the API