Using SolidEdgeFileProperties.PropertySets without SE installed

Valued Contributor
Valued Contributor

 

I have a program that reads and updates Solid Edge file properties using SolidEdgeFileProperties.PropertySets.

I'd like to be able to use this program on computers that do not have a full installation of Solid Edge.  Is this possible and if so what do I need to do?

Thank you.

Carl Breving

 

Posted by: Carl Breving
Post date: 3/24/2010 5:30:48 AM

3 REPLIES

RE: Using SolidEdgeFileProperties.PropertySets without SE installed

Valued Contributor
Valued Contributor

Carl,

 

We have done this here, but installing these files, in this directory structure.

These files were originally found in the "C:\Program Files\SolidEdge V20\Program" directory.

 

C:\SolidEdge_v20_API\PropAuto.dll

C:\SolidEdge_v20_API\ResDLLs\0009\jdocres.drx

 

After copying into place, we then register it using:

regsvr32 "C:\SolidEdge_v20_API\PropAuto.dll"

 

Its worked for us, but I'm not sure if you will require different ResDLLs (presumably language related).

 

Thanks,

Chris.

 

Posted by: chris mann
Post date: 3/24/2010 6:03:49 AM

RE: Using SolidEdgeFileProperties.PropertySets without SE installed

Valued Contributor
Valued Contributor

 

Chris.

That worked perfect.  The part I was missing was the \ResDLLs\0009\jdocres.drx

Once I added that I was able to register the PropAuto.dll and run the program.

Thank you.

Carl

 

Posted by: Carl Breving
Post date: 3/24/2010 6:14:53 AM

RE: Using SolidEdgeFileProperties.PropertySets without SE installed

Valued Contributor
Valued Contributor

 

One note that I also needed \ResDLLs\0009\PropMgr.drx in order to use some of the other properties like Template.

 

Posted by: Carl Breving
Post date: 3/25/2010 7:01:17 AM