Cancel
Showing results for 
Search instead for 
Did you mean: 

Variable table

Creator
Creator

Hello Everyone,

 

I have a question about the variable table.

Is there a way to modifiy the variable table just like the file properties without opening the Solid Edge file?

 

Then later when you open that file the file will update to the latest value in the variable table.

 

Thanks

 

Teus

2 REPLIES 2

Re: Variable table

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

HI Teus,

 

jein, you can modify only the existing variable.

you need Microsoft Excel for that. Select the value in Excel, copy that, then in Solid Edge variable table Right click on Formula cell and select past link. In this case you can modify this variable in Solid Edge, if you change the value in Excel.

 

Note: you should not change the path of this Excel

you can modify only the locked dimension.

 

Tripi

Re: Variable table

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi @Tripi,

Sending values from Excel to Solid Edge will need to run both programs on your computer. This is done by COM (also known also "object linking an embedding" , OLE) . Excel will send data to Solid Edge, which the will write the value to the variable.

So Solid Edge has opened the file in question.

File properties are stored in a well known format in a sub section of the .par file. This is defined by Microsoft and is equivilent to the information in excel or word files. As a consequence windows explorer can show information like title or author without Solid Edge installed on the computer.

regards

JB
SE 2019, VS2017