Visual basic and free Solid-Edge 2d

Pioneer
Pioneer

Hello

I try to modify Custom Property using Excel and Visual Basic.

My customer his using a free 2d Solid-Egde.

First I check for SE to be running

 

.....

On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application")

If Err Then

MsgBox "Solid Edge must be running"

Else ....

 

Here no problem Solid-Edge is running OK.

 but when I try to modify custum property whit the code

 

checked_date = Left(DateTime.Now, 10)

' Connect to Solid Edge Set IApp = GetObject(, "SolidEdge.Application") '***************************************************************************

'Access the CustomInformation properties collection

Set objInfoPropSet = objProp("Custom")

'************************************************

Set objProperty = objInfoPropSet("_checked_date")

If Err Then Set Prop = objInfoPropSet.Add("_checked_date", "checked_date")

End If

Set objProperty = objInfoPropSet("_checked_date") 'Adjust the value

objProperty.Value = checked_date

 

nothing appens in the dft.

 

Works fine using Solid-Edge fondation

 

Any idea

 

Thank, merci

Phil

 

 

4 REPLIES

Re: Visual basic and free Solid-Edge 2d

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I'm not sure if it is still this way but I recall in the past that the API was not made available in the free edition. Can anyone confirm?

Jason Newell
Applications Architect
www.jasonnewell.net

Re: Visual basic and free Solid-Edge 2d

Pioneer
Pioneer
Hi
You are rigth. To bad. Thank
Phil

Re: Visual basic and free Solid-Edge 2d

Phenom
Phenom

This is a real shame - we have a guy who does wiring diagrams etc that are often just conversions from other systems (Microstation, AutoCad) and the free 2D version would be ideal. Unfortunately he can't use any of the macro's that we have for placing drawing borders etc.

HP Z420 16GB RAM
Quadro K4000
ST10 MP3 on Windows 10 Pro 64.

Re: Visual basic and free Solid-Edge 2d

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Did you install Solid Edge from the DVD or from the free 2D download link.

 

I have customers that use macro with the free 2D version, they just install SE with the DVD and use the Free 2D licence file.


Romuald BERTIN