Cancel
Showing results for 
Search instead for 
Did you mean: 

Wanted - SE Draft Styles

Valued Contributor
Valued Contributor

I am seeking some help locating the correct API calls for draft styles. I am looking to have my program call the draft styles from one draft and then change the styles in another. I have no problem swapping drafts but just need help with the API's for the styles. I need code to pull the Text, Caption, and Callout styles and then the code to set them. I am coding in C# .net 4.0 but code in VB would be fine as well.

 

I have looked into the object TextStyles but all the information I can get is the default name but no text font or size.

 

Any help is much appreciated.

 

SE ST5 MP03

 

Thank you

 

Posted by: Jamie Griffis
Post date: 3/5/2013 11:22:11 AM

1 REPLY

Wanted - SE Draft Styles

Valued Contributor
Valued Contributor

Did you have any luck finding how to do this? We also need to do the same thing.

 

Posted by: Carl Breving
Post date: 3/19/2013 3:43:20 PM