What does the Status in SolidEdgePart.WeldmentModel.GetPhysicalProperties mean?

Creator
Creator

Hello,

 

I looked it up in the ST7 Documentation and it says:

"StatusReturns the status of the physical properties of the model. The physical properties can be non-existent, out-of-date, or up-to-date."

The return value of Status is an integer so I assume that the Status can be 0,1 or 2 but what value stands for wich status?

 

Kind regards,

Loginator

2 REPLIES

Re: What does the Status in SolidEdgePart.WeldmentModel.GetPhysicalProperties mean?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Hi,
you get Status=1 if the values are up-to-date and Status=2 if out-of-date.

I never got other values, since an exception is raised, if there is no model or user defined values.
You should also check if there is a realistic density defined.
regards

JB
SE ST10

Re: What does the Status in SolidEdgePart.WeldmentModel.GetPhysicalProperties mean?

Creator
Creator
Thanks for the answer Smiley Happy