Cancel
Showing results for 
Search instead for 
Did you mean: 

Which version for VB

Valued Contributor
Valued Contributor

 

Hello,

I'm an absolute beginner...

I want to make some simple buttons with simple code behind them.

Can i do this with the version VB for applications that is shipped with Microsoft Office, or do i need another version. Are there some free version?

Thanks, Johan

 

Posted by: johan degreef
Post date: 1/7/2008 12:47:37 AM

1 REPLY

RE: Which version for VB

Valued Contributor
Valued Contributor

The quickest & cheapest way to get up and running I think is to download the Express version of VB.NET. The following link used to work for 2005 edition but it's been replaced with 2008. You may have to do some hunting if you want 2005.

 

http://www.microsoft.com/express/vb/

 

Posted by: Jason Newell
Post date: 1/7/2008 2:28:28 PM