Cancel
Showing results for 
Search instead for 
Did you mean: 

XRoute and BendTable

Valued Contributor
Valued Contributor

 

Hi,

I have an XRoute and I want to get information about its tube, such as  diameter, start point, end point etc....

(The same info that you can get from Tools->BendTable in SE.).

 

SE provides BendTable method, but it can be applied on SheetMetalDocument. Is there any way to get a SheetMetalDocument object  of XRoute?

 

I can get TubeFeature from the XRoute, but I can't apply a BendTable method on it. Is there a way to get the desired information from about the tube from the TubeFeature not using the "BendTable" method?

 

Thank you.

Any help will be appriciated.

 

 

Posted by: Baba baban
Post date: 11/26/2008 4:11:48 AM

1 REPLY

RE: XRoute and BendTable

Valued Contributor
Valued Contributor

you can see Tube..::BendTable Method it may help you

 

Posted by: anil upmanyu
Post date: 1/11/2009 8:30:43 PM