Cancel
Showing results for 
Search instead for 
Did you mean: 

Zone created with API not working

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi all,

 

I have created zones with API but those zones doesn't display any parts of my assembly.

 

Here is my code :

    Public Function CreateZone(ByVal ObjDoc As SolidEdgeFramework.SolidEdgeDocument, _
                               ByVal ZoneName As string, _
                               ByVal Interference As boolean, _
                               ByVal P1X As Double, _
                               ByVal P1Y As Double, _
                               ByVal P1Z As Double, _
                               ByVal P2X As Double, _
                               ByVal P2Y As Double, _
                               ByVal P2Z As Double, _
                               ) As Boolean
        CreateZone = True

        Try
            Dim Zones As SolidEdgeAssembly.Zones = ObjDoc.Zones

            Dim a_Zone As SolidEdgeAssembly.Zone = Zones.Add(P1X, P1Y, P1Z, P2X, P2Y, P2Z)
            a_Zone.Name = ZoneName
            a_Zone.Overlap = Interference
            a_Zone = Nothing

        Catch ex As Exception
            CreateZone = False
        End Try
    End Function

 

Can you help me with this problem ?


Romuald BERTIN
2 REPLIES

Re: Zone created with API not working

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Romuald,

 

I am on ST 6 and it is working for me partially.

The zone box appears but the zone name does not appear in the zone tree node.

I switched to a different tab and back to the Select Tools tab to get the zone name listed under the zones tree node. I believe this could be the reason for even a_Zone.ShowOnlyParts() and objDoc.UpdateAll not to work.

 

Regards,

Tushar Suradkar

 

Re: Zone created with API not working

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thanks Tushar for those infos.

 

I'm in ST7 and the zone are correctly displayed in the graphic window and in the zone treenode.

 

There seems to be problem when calculating, maybe by a query, the components taht match the zone so it doesn't display anything.

 

If I select a zone then modify its definition and change the size in Solid Edge then it display correctly the components.


Romuald BERTIN