Cancel
Showing results for 
Search instead for 
Did you mean: 

activeX viewer without SE installed

Valued Contributor
Valued Contributor

Bonjour !!!

Good morning every one,

thanks Jason for your site.

My Access VBA macro launches a SEDraftX activeX to show results in a query form. It works well but I need to install SE on every workstation, even if un-needed. To avoid this, I tried to manually regsvr32 a local copy of the SEDraftX.ocx instead of install a full SE.

DOS line hereafter

c:\program files\solid edge V18\program>regsvr32 SEDraftX.ocx

 

Does anyone have a way or a turn around to use a SE activeX without installing a full SE?

 

regards

 

Posted by: Ludovic BOUILLON
Post date: 6/22/2006 7:58:19 PM

3 REPLIES

RE: activeX viewer without SE installed

Valued Contributor
Valued Contributor

Ludovic,

 

All you need is the free viewer.

 

http://www.solidedge.com/viewers

 

Posted by: Jason Newell
Post date: 6/23/2006 12:35:53 AM

RE: activeX viewer without SE installed

Valued Contributor
Valued Contributor

Dear Jason,

merci (thanks) for your answer.

You're right, my VB6 macros using SE activeX do work only with the viewer installed.

I just wonder why my Access VBA macro doesn't ... it needs a full SE install.

I'm going to develop again that small Access macro on a workstation without SE installed, only SE Viewer ... to see if it behaves better.

 

cordialement

Regards

 

Posted by: Ludovic BOUILLON
Post date: 6/29/2006 3:35:08 AM

RE: activeX viewer without SE installed

Valued Contributor
Valued Contributor

Ludovic,

 

I can't imagine why you would need full SE for that to work. The viewer components are (should be) the same if you install just the viewer for full SE. If you can't get just the viewer install to work in Access, I guess I just don't know the answer.

 

Good luck!

 

Posted by: Jason Newell
Post date: 6/30/2006 5:35:46 AM