Cancel
Showing results for 
Search instead for 
Did you mean: 

arrays

Valued Contributor
Valued Contributor

Hello,

I am try to convert over to NET from VB 6, I have some arrays from VB6 that were variant, when I converted them

to NET they went to objects. For example:

 

dim dblarray as object (which was variant in VB6)

dim strname as string

dim introw as integer

 

strname = "A/R"

 

dblarray(intRow, 4) = name

 

I get this error

An unhandled exception of type 'System.InvalidCastException' occurred in microsoft.visualbasic.dll

 

Additional information: Cast from string "A/R" to type 'Double' is not valid.

 

it worked in VB6, how do I fix this, any help would be appreciated

thanks

Paul Martz

National Steel Car

905-544-3317 ex 3341

 

Posted by: Paul Martz
Post date: 11/4/2005 1:21:58 AM

1 REPLY

RE: arrays

Valued Contributor
Valued Contributor

Hi Paul,

 

In .Net you have to be a bit more specific about arrays.

Try something like this

 

Dim dblArray(1, 1) As Object

 

This creates a 2-Dimensional Array of Objects with 2 element in each dimension - 4 Elements in total dblArray(0,0) dblArray(0,1) dblArray(1,0) and dblArray(1,1).

 

to redefine the array use ReDim making sure to use Preserve if you want to keep the existing content e.g.

 

ReDim Preserve dblArray(2,2) 'Now the array has 3 elements in each dimension.

 

Hope this helps

Calum

 

Posted by: Calum McLellan
Post date: 11/6/2005 7:06:52 AM