Cancel
Showing results for 
Search instead for 
Did you mean: 

i want program in positon solid edge

Valued Contributor
Valued Contributor

 

 

 

i want program in positon solid edge

how???

 

Posted by: kim sunil
Post date: 1/7/2010 3:47:19 PM

3 REPLIES 3

RE: i want program in positon solid edge

Valued Contributor
Valued Contributor

An impossible Programming ?????

 

Posted by: kim sunil
Post date: 1/11/2010 9:16:55 PM

RE: i want program in positon solid edge

Valued Contributor
Valued Contributor

I believe the sdk directory has a sample vb.net addin that has a command that adds a dialog to the command bar. Pretty sure the VC++ sample add-in does to (I posted it on this site a while back and it should be in the V102 sdk).

 

Posted by: R.D. Holland
Post date: 1/26/2010 4:57:38 AM

Re: i want program in positon solid edge

Valued Contributor
Valued Contributor

vb.net code

 

Dim x as double = nothing

Dim y as double = nothing

dim z as double = nothing

 

<occurence object>.getorigin(x,y,z)

 

This x,y,z gives the position of the occurence with respect to the relative assembly in which it exists....

 

 

I need the code to get the position of the occurence with respect to the main assembly...

PLEASE HELP ME OUT ....................... Smiley Sad

 

Posted by: Jacob Andrews
Post date: 9/14/2012 10:44:51 AM