Cancel
Showing results for 
Search instead for 
Did you mean: 

is it possible to Select all entity in draft sheet through solidedge automation

Pioneer
Pioneer
hi, i have to select all entities, copy and paste it to the another sheet (i found few more post same like my one. but i could not found the answer on that). i used selectset method mentioned in this forum and few more. But it is not working. and i tried group all entity and than copy and paste also. this one also not working. is it possible. if possible please share the code... thanks, balaji.l
1 REPLY

Re: is it possible to Select all entity in draft sheet through solidedge automation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi, happy new year...

There is a AddAll method in the SelectSet object. This should put all element on the active sheet to the SelectSet.

Look in the SDK help to find example code.

After adding the elements to the select set, you can use Copy() method to add them to the windows clipboard.

 

regards

JB
SE ST10