Cancel
Showing results for 
Search instead for 
Did you mean: 

launch bottoms from tool bar

Valued Contributor
Valued Contributor

Hi,

I'm looking for a way to launch the operation which is called when clicking on extrude.

Yes I saw in the documentation that it works on an object , yet I would like to know to do that even without any object - it is possible to click on extrude from menu in part env' without any thing..

This is what I'm looking for a way to do.. is there a way to launch events to the solid edge or to call extrude procedure as if the menu was pressed?

 

Posted by: joseph polk
Post date: 3/15/2012 3:09:18 PM

1 REPLY

Re: launch bottoms from tool bar

Valued Contributor
Valued Contributor

solved using SolidEdgeFramework.Application as a StartCommand method.

 

Posted by: joseph polk
Post date: 3/18/2012 7:08:09 AM