Showing results for 
Search instead for 
Did you mean: 

logging user actions

Valued Contributor
Valued Contributor


Hi to all,

     i'm new in programming solidedge and so i'm sorry if i'm asking something too simple. I installed the wizard for creating addins and i found example files extremely useful!

But i have to code a strange addin: i've to catch  and, initially log only, all  the actions an user could perform on a sketch or similar, such as extrusions, revolves, holes and so on. Until now I am able to catch all application, application_window, addin and fileui events thanks to Jason example. But these ones aren't so useful for me (i don't even know the corrispondance between commandid and commandname): my aim is to log all user actions with relative action parameters and attributes. For example: extrusion on sketch1, height 20 cm, direction z-axis. Is there any way to achieve this? Can you put me on the right direction?

Any help would be very appreciated!

Many thanks in advance,



Posted by: Villa Enri
Post date: 7/24/2009 3:29:05 AM


RE: logging user actions

Valued Contributor
Valued Contributor



I'm sorry to tell you that the Solid Edge API is not that robust. If it were, we would have already written a macro recorder by now.


Posted by: Jason Newell
Post date: 7/24/2009 10:12:26 AM