Cancel
Showing results for 
Search instead for 
Did you mean: 

re-sizing window for SaveAsImage in Draft

Valued Contributor
Valued Contributor

The end result I want is an image of a draft where the image only includes the area within the borders defined by the sheet setup height and width.

To accomplish this, my idea was to get the size from the sheet setup, move the sheet to the top left corner of the viewing window, and then resize the window to the size of the sheet and take the picture. The code below does what I want until the last step of resizing the window. I have tried all the ways I can think of that might work using Application.Windows or as shown below using the Draft.SheetWindow object, but I either get errors or it just doesn't work. Does anyone know how to accomplish that last step, or is there a better way to go about this altogether? Thanks!

 

Dim objApp As SolidEdgeFramework.Application = Nothing
Dim objDraft As SolidEdgeDraft.DraftDocument = Nothing
Dim objSheet As SolidEdgeDraft.Sheet = Nothing
Dim objSheetSetup As SolidEdgeDraft.SheetSetup = Nothing
Dim objSheetWin As SolidEdgeDraft.SheetWindow = Nothing

' Connect to a running instance of Solid Edge
objApp = Marshal.GetActiveObject("SolidEdge.Application")

' Get a reference to the active document
objDraft = objApp.ActiveDocument

' Get a reference to the first sheet
objSheetWin = objDraft.Windows(0)
objSheet = objDraft.ActiveSheet
objSheetSetup = objSheet.SheetSetup

' Set the sheet to fit the screen
objSheetWin.FitEx(SolidEdgeDraft.SheetFitConstants.igFitWorkingAndBackgroundGraphics)
' Move the sheet to the upper left corner of the screen
objSheetWin.SetOrigin(0, objSheetSetup.SheetHeight)
' Set the window so that it is not maximized, and therefore can be re-sized
objApp.WindowState = System.Windows.Forms.FormWindowState.Normal

Dim factor As Double = 39.3700787402 * 72 ' meters to inches * 72 dots per inch
' this code does not work (no re-sizing occurs at all):
objSheetWin.Height = objSheetSetup.SheetHeight * factor
objSheetWin.Width = objSheetSetup.SheetWidth * factor

' Save the current view as an image
objSheetWin.SaveAsImage("C:\Users\tim\Desktop\testdraftimage.jpg")

 

Posted by: Tim
Post date: 6/20/2012 10:50:59 AM

1 REPLY

Re: re-sizing window for SaveAsImage in Draft

Valued Contributor
Valued Contributor

You must set the viewer windowstate to normal

objSheetWin.WindowState = System.Windows.Forms.FormWindowState.Normal

and not objApp.WindowState

 

Regards

JR

 

Posted by: JR
Post date: 6/21/2012 7:12:45 AM