Cancel
Showing results for 
Search instead for 
Did you mean: 

reading sesnsor value

Valued Contributor
Valued Contributor

 

HI all

I have placed surface area sensor on to faces of a part.

the reading i can see in sensor window.

how can i write this data in a file.

secondly two sensor are placed on ends (faces)

I need 2 more in between but as there is no face so how can i put a sensor .

is it possible that i define a plane and some how place a sensor on it , and it can calculate the crossection area?

help required

Regards

Ali

 

Posted by: ali kamran
Post date: 12/13/2009 1:30:54 AM

1 REPLY

RE: reading sesnsor value

Valued Contributor
Valued Contributor

Hi

I would also like to know this

 

/Per

 

Posted by: Per Norlander
Post date: 1/19/2010 11:53:32 PM