Cancel
Showing results for 
Search instead for 
Did you mean: 

sketch index count reset

Is there a way to reset the indexing counter for features, such as sketches, protrusions, cutout, etc...

 

I have a file we want to use as a template but this file had some feature creation in the past.

 

If we save it as the template and then use it  the 1st sketch begins with "Sketch 5" and "Protrusion 3"

 

Is there any exposure via the API to reset these indexes?

2 REPLIES 2

Re: sketch index count reset

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Not that I know of or can find. 

Jason Newell
Solutions Architect
www.jasonnewell.net

Re: sketch index count reset

GTAC advised that this is stored in the part file itself and not exposed via API.

 

logged as ER