Cancel
Showing results for 
Search instead for 
Did you mean: 

what OAF file in Teamcenter and how to create through the API

Experimenter
Experimenter

I have created a SE Part data set using Solid Edge and SEEC. In I Tc I see a .par file along with it .qaf file, what is it and how to creates using API

I have added SE Part using ITK and I do not QAY is create and image file , how to do that using API’s

 

Thanks,

Sreedhara Reddy Avula

2 REPLIES

Re: what OAF file in Teamcenter and how to create through the API

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Sreedhar,

you have to use the SEEC part in the Solid Edge API. There are several methods in the SolidEdgeTCE object.

Look here

http://support.industrysoftware.automation.siemens.com/training/se/107/api/webframe.html

 

You could use the CheckInDocumentsToTeamCenterServer() method to add a File as Dataset to an existing Item. Bee shure that the file properties are filled with the right information!

 

Regards Jürgen

regards

JB
SE ST10

Re: what OAF file in Teamcenter and how to create through the API

Experimenter
Experimenter

Thanks JB, I am alreday using this method, I am facing problem when I use this API. I am not getting all links(intra part links) and also if I upload an assembly and if it has an subassembly , it is not uplaoding subassembly.

 

Thanks,

Sreedhar