Cancel
Showing results for 
Search instead for 
Did you mean: 

2-D Rectangular Pattern

Experimenter
Experimenter

I'm fairly new to Solid Edge, and I can't figure out how to create a 2-D rectangular pattern of an ellipse. I need one column of 25 ellipses. Clicking on the ellipse before I select rectangular pattern hasn't worked for me. I'm also using a trial version, if that helps. Thanks in advance!

3 REPLIES

Re: 2-D Rectangular Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Here is a video showing how it works.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: 2-D Rectangular Pattern

Experimenter
Experimenter

I noticed that video shows it done in the drawing template. I tried doing what was shown in Sketch mode of the part template and it didn't work. Is there a difference between the two templates?

Re: 2-D Rectangular Pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Yes, they have different functions, based on the environment [Template] you're in.

By "2D pattern", Ken, as did I, thought you meant the "Draft" environment of SE...if you are designing a 3D model, then the appraoch is slightly different.

 

The sketch mode of the "Part" environment, SE uses the sketch geometry to be the basis of the patterns for design feature[s] to reside in a 3D model document, or complete model[s] in the "Assembly" environment. So the first instance of the pattern needs to exist first.

 

Whereas, sketching in the "Daft" environment, is all about the sketch geometry, and patterns act on it accordingly....as per Ken's video.

 

HTH.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019