Cancel
Showing results for 
Search instead for 
Did you mean: 

2 setups for property manager

Pioneer
Pioneer

hi,

is it possible, 2 have 2 different setups, for the property manager?

i want one, for parts produced inhouse, with the needed properties.

and the another one, for ex. imported parts (bolts, washers etc.)

 

Best regards

Brian Nielsen

Semvac A/S

Denmark

Best regards

Brian Nielsen
Wabtec
4 REPLIES

Betreff: 2 setups for property manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Bravo

 

 

due to the fact that the Prop Manager settings are stored witin the registry of the Current user, You can export setting one and setting two one after the other and use those reg files to change Your Property Manager by clicking them from explorer.

Of course this might not be the most elegant way but it would be a working solution!

 

regards
Wolfgang

Re: 2 setups for property manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Do you want this because if you include all the property columns for both it's too many columns and hard to work with?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: 2 setups for property manager

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

HI @Bravo

 

 

 

this is a very good point by @bshand

 

The property manager itself is a very good tool, but the interface with many columns from left to right makes it difficult to use.

This also is or was a reason that I rogrammed a "Property Manager" for my own use by myself.

 

20171115_1924.PNG

regards
Wolfgang

Re: 2 setups for property manager

Pioneer
Pioneer

hi,

@bshand yes it's mostly because of all the colums.

and for the imported parts, we only need a few of them.

 

@hawcad i would love to make my own manager, with the overview, and properties needed.

but i have no idea, how and where to start. so the SE manager, will have to do the job for now.

 

Best regards

Brian Nielsen
Wabtec