Cancel
Showing results for 
Search instead for 
Did you mean: 

24 h download link problem!

Not applicable

I registered to the Siemens' site with the mail of my university to download the free student version of Solid Edge ST6. The download was very slow so I waited a day.
The problem is that the download link lasts only 24 hours and now it's invalid, and I can't download the program anymore.
What can I do?

1 REPLY 1

Re: 24 h download link problem!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Register again and use a download tool like Download Accelerator Plus.
Sent from my Motorola Electrify using Tapatalk 2


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com