Cancel
Showing results for 
Search instead for 
Did you mean: 

2D Draftsight Drawings Transfer to Solid Edge

N/A

I started to learn on 2D DraftSight and have drawings on file. I would like to know how to transfer these drawings onto Solid Edge.

Thanks
Crousie

3 REPLIES

Re: 2D Draftsight Drawings Transfer to Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Use the Open command in Solid Edge and change the "File of type" filter to DWG. Specify a DFT template if asked.


Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: 2D Draftsight Drawings Transfer to Solid Edge

N/A
I found the drawing on DraftSight with the drawing done, opened it and finding the dimensions are missing as well as some of the text is missing.
The drawing was bigger than the screen... hit fit the screen went to a minuet drawing. Had to hit zoom to area many times, to even evaluate it.

Re: 2D Draftsight Drawings Transfer to Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Crousie,
I expect there is a scaling issue going on here, upon import......when you are browsing for the file to open into Solid Edge, before you choose to open it, have a glance at the "Options" button and there will be some things to adjust to your requirements. Dimensions and other text may/may not come in cleanly from that "other" product, but it's very easy to just place new ones. Smiley Very Happy
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000