Cancel
Showing results for 
Search instead for 
Did you mean: 

2D Free and SE Viewer

Gears Phenom Gears Phenom
Gears Phenom

I installed the free 2D version of Solid Edge on the PC of my colleague.

I was surprised the installation is identical to mine, the only difference is the license file.

 

But the biggest surprise came after that.

 

He can open 2D files, but can't view 3D! Therefor he needs the viewer, but...

You can't install the viewer next to Solid Edge...

 

Why can't the free 2D version have the functionality like the viewer?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
10 REPLIES

Re: 2D Free and SE Viewer

Phenom
Phenom
Solid Edge Viewer is part of Solid Edge Installation.
Just have a look in the start menu.
Highlighted

Re: 2D Free and SE Viewer

Gears Phenom Gears Phenom
Gears Phenom

I mean, When you open a draft, you see views of parts and assembly's.

Why can't he just open the part/assembly/sheet metal by double click on the view, just like in the full installation?

Just open the file and look, nothing more.

 

I fully understand it is free, so you can't have full functionality, but why not the best of 2 free versions together?

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: 2D Free and SE Viewer

Phenom
Phenom

I was answering at this sentence:

 


@Joris wrote:

But the biggest surprise came after that.

 

He can open 2D files, but can't view 3D! Therefor he needs the viewer, but...

You can't install the viewer next to Solid Edge...


You can't install the viewer because it is already installed

 

About this:

 


@Joris wrote:

I mean, When you open a draft, you see views of parts and assembly's.

Why can't he just open the part/assembly/sheet metal by double click on the view, just like in the full installation?

Just open the file and look, nothing more.

 

I fully understand it is free, so you can't have full functionality, but why not the best of 2 free versions together?


I agree it would be great but maybe not everybody would like a full installation just to view files.

Anyway about the reasons only Siemens can answer.

 

 

Re: 2D Free and SE Viewer

Gears Phenom Gears Phenom
Gears Phenom

Thanks for thinking with me.

 

So I went to the PC of my collegue.

I double clicked on an assembly: SE free 2D opens. Why?? SE free can't handle this file.

So I changed the "open with" for asm files to the viewer. Ever tried to find the exe? It's well hidden.

 

Now the icon for an asm file is the same as a txt file.

 

How do I have to explain this to someone who can barely work with a computer?

 

So my suggestion is:

 

1: People install SE free 2d

SE is installed, draft has full functionality for dft (like now) and viewer functionality for the rest.

double click on a drawing view opens the part/assembly/...

 

2: People only want to view

They install the viewer like it is now.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: 2D Free and SE Viewer

Valued Contributor
Valued Contributor

Is it still true that you cannot have the Free 2D drafting pkg loaded and run the 3D viewer?  We have user (Mfg engr) that uses the viewer to see the models in order to assist them with the creation of BOM & RTG's.  They also need the free 2D dft for obtaining surface area, lengths, and more to establish qt'y info for the BOM's.  

 

This has been a big inconvienience for us.  We have floating license's, but they really don't need a full version of Solid Edge for what they do.  Any options?

Re: 2D Free and SE Viewer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe the seviewer is installed but no Start menu entry for it with ST9.

 

Located here:

C:\Program Files\Solid Edge ST9\Program\win32



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: 2D Free and SE Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

The seviewer is not installed with base ST9.  The seviewer is now installed with MP1 and higher and there is no start menu created.

Re: 2D Free and SE Viewer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And if using Free2D, no MP's unless you are under maintenance... correct?



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: 2D Free and SE Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

Correct!  If you do not have any Solid Edge maintenace (for any product) then you will not have access to maintenance packs if running Free 2D only.