Cancel
Showing results for 
Search instead for 
Did you mean: 

2D drawing views not showing the hidden lines

Experimenter
Experimenter

problem.png

My drawing isn't showing the hidden lines.

What should I do? Thanks a lot.

3 REPLIES

Re: 2D drawing views not showing the hidden lines

Esteemed Contributor
Esteemed Contributor

Hi there @Vbelemf,

 

Is this a draft of 3D models, or are they 2D sketched views only?......the steps are different, depending on which they are.

 

OK, so hopefully they are linked to the parent model [ASM in this case]....so what you need to do now, is select one of the views, then, either right click, or pick from the ribbon bar, the "Properties" command, and select to display hidden lines......repeat for other views, and update views when done.

 

If you know you want views this way at the time of selecting the model, you can configure it before actually placing the views, using the Drawing View Wizard - Options.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: 2D drawing views not showing the hidden lines

Experimenter
Experimenter

Hi Sean,
Thanks for the response.
It's a 3D model assembly that I transformed into 2D viewsdrawing.png

Highlighted

Re: 2D drawing views not showing the hidden lines

Experimenter
Experimenter

Worked like a charm,

I just had to update the drawings.

Thanks a lot again.