Cancel
Showing results for 
Search instead for 
Did you mean: 

2D line offset

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I want to draw in 2D a device which consists of many parallel, offset lines.  It is annoying that I have to then go back and delete the offset distance dimmensions and the offset symbol on each of many offsets. Is there a way to change this?

2 REPLIES

Re: 2D line offset

Genius
Genius

dgalitzine, have you tried the array command. Look under HOME/MIRROR/RECTANGULAR PATTERN.  The command requires that you draw one line where you want it with a set length.  The balance of the command lets you set the offset distance in both x and y (i.e., if applicable) directions. No dimensions show up in the result.

 

Ron

Re: 2D line offset

Valued Contributor
Valued Contributor

If you turn off "maintain relationships" while you use the offset command you will not get the dimensions.

If you do end up with lots of dimensions you can use quick select and delete then all at once.

 

Pete