Cancel
Showing results for 
Search instead for 
Did you mean: 

32bit or 64bit

N/A

i have a 64 bit, and i registered to download the software, however they sent me a download link to a 32bit program. is there a 64bit i can download, and what are the specs to run this program on my pc?

2 REPLIES

Re: 32bit or 64bit

Phenom
Phenom
I don't know if a 64 bit program for students available to download, but there are very few advantages of a 64 bit install over 32 bit unless you are working with MASSIVE draft files/assemblies. So, rest easy.
-Dylan Gondyke

Re: 32bit or 64bit

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Student version is 32 bit only which will operate just fine on a Windows x64. As Dylan said, there is no advantage unless working with massive assemblies.


Ken

Production: ST10 MP6
Testing: SE 2019