Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Measure ( Measure - Distance Type ) Not clickable / Not Available

Experimenter
Experimenter

Hello Solid Edge Community,

 

I seem to have a problem with my 3D Measure (Distance Type).

It doesn't seem to be available when I try to use it and only displays Total Distance without a value (0.00mm).

 

I tried to test it on to my laptop and it works fine but my laptop isn't compatible with Solid Edge since it has the GTX Card (failed to do a thorough research with choosing a laptop for CAD applications). I need to fix this on my desktop.

 

Do you have any recommendations?

 

Here is a screenshot:Query.png

 

 

2 REPLIES

Re: 3D Measure ( Measure - Distance Type ) Not clickable / Not Available

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Check your Keypoint filter.  It is currently set to "Endpoint" only and may be the issue...

2017-04-27_11-08-08.png

 



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: 3D Measure ( Measure - Distance Type ) Not clickable / Not Available

Experimenter
Experimenter

Thanks! It's solved.