Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Sketch from AutoCAD

Legend
Legend

Now that we have 3D sketching is there any way to take a 3D ACAD wireframe and import it as a 3d sketch?

Using SE since V12, 2002
ST10 certified
3 REPLIES 3

Re: 3D Sketch from AutoCAD

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Larry,

 

Not that I'm aware of, as yet......you'd still need to created solids along the wireframe paths to send to Solid Edge.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: 3D Sketch from AutoCAD

Phenom
Phenom

Just an idea - if you export as an iges file from AutoCad can you then import curves into Solid Edge?

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: 3D Sketch from AutoCAD

Legend
Legend
I submitted a PR, now it is ER 7261907 to open a 3D dxf in part or assembly as a 3D sketch.
Using SE since V12, 2002
ST10 certified