Cancel
Showing results for 
Search instead for 
Did you mean: 

3Dconnexion 10.5.0 driver released... With rotation option for sketch/profile!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

3Dconnection has posted an updated driver (10.5.0) that has an option to disable rotation in sketch/profile.

 

https://www.3dconnexion.com/index.php?eID=sdl&ext=tx_iccsoftware&oid=93e0cc8a-cb0b-11df-607c-598a0e7...

 

2017-08-11_11-22-55.png



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com
2 REPLIES

Betreff: 3Dconnexion 10.5.0 driver released... With rotation option for sketch/profile!

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

 

I already have downloaded this driever today morning and updated my installation.

 

And Yes now the old fashioned setting for profile is available again.

 

And Yes, You are absolutely right to post this info here in the forum.

 

Sorry for do not when finding it.

 

Kudo for You Kenny

 



regards
Wolfgang

Re: 3Dconnexion 10.5.0 driver released... With rotation option for sketch/profile!

Phenom
Phenom

Just when I thought i started to like it being able to rotate..

   I often have to rotate the part to see whats "behind" the profile I'm sketching or if I'm "including" an edge/sketch to be sure I'm selecting the correct one. If I need to lock to the plane I'll simply click the "lock rotation" button on the 3D mouse (space mouse pro). I also have a button programmed to "Ctrl-H" to quickly return to sketch profile, and another for "Ctrl-Q" to show/hide previous levels.

-Craig