Cancel
Showing results for 
Search instead for 
Did you mean: 

3d views don't work. Solid Edge keeps using canonical display driver.

Experimenter
Experimenter

I can't use any 3d modelling stuff(part, sheet, assembly...), draft works fine. As soon as click on parts it crashes. Crash log indicates that it was using canonical display drivers. I've Intel HD 4000 and drivers for same are installed on system. How to force solid edge to use Intel drivers. It works with intel hd 4000, i know that. 

Capture.PNG

p.s - I am running SE on windows 10 10240

3 REPLIES 3

Re: 3d views don't work. Solid Edge keeps using canonical display driver.

Hi nemesis,

 

I think your problem is "not have correct MP for solid edge "ST7" because need MP4 on windows 10".

 

Tibor

Re: 3d views don't work. Solid Edge keeps using canonical display driver.

Experimenter
Experimenter

Okay. I'll update it Smiley Wink Thanks!

Re: 3d views don't work. Solid Edge keeps using canonical display driver.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there, Also....Solid Edge is not supported for Windows 10 yet, especially on any unofficial versions.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000