Cancel
Showing results for 
Search instead for 
Did you mean: 

64 bits problem

N/A

Right now im downloading the student version and it says is 32 bits but my pc wirks at 64...I can use it without problem or not

6 REPLIES

Re: 64 bits problem

N/A
Yes, it will work fine on a 64 bit machine.
Ken
http://grundey.blogspot.com
http://www.pella.com

On 9/23/2011 11:58 PM, alejandro.cardona.velez@gmail.com wrote:
> Right now im downloading the student version and it says is 32 bits but
> my pc wirks at 64...I can use it without problem or not
>
>

Re: 64 bits problem

N/A
Hello,
question @Bione PLM
Is there a reason why the 64bit version is not available? As far as I know the academic version from our university is 64bit, too.
Thank you

Re: 64 bits problem

N/A
I'm guessing simplicity. One download for your chosen language that
works on both 32 and 64 bit Windows. Why complicate it with a 64 bit
version too if it is not necessary?
Ken
http://grundey.blogspot.com
http://www.pella.com

On 9/27/2011 1:48 PM, sb82@rz.fh-augsburg.de wrote:
> Hello,
>
> question @Bione PLM
>
> Is there a reason why the 64bit version is not available? As far as I
> know the academic version from our university is 64bit, too.
>
> Thank you
>
>

Re: 64 bits problem

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
Ken is correct.

We took the decision to make it as easy as possible for Students to obtain and use Solid Edge. The Solid Edge University Edition is available in both 32 and 64 bit and schools, colleges, and universitiy customers using the University Edition can make it available to their students.

But for the Student download we standardised on the 32bit.

Re: 64 bits problem

N/A
Hello I downloaded solid edge student version but when I am going to extract this files it show me an error. what can I do?

Re: 64 bits problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hello I downloaded solid edge student version but when I am going to extract this files it show me an error. what can I do?


Hi there,

Could you give a little more detail on the error you're seeing?
If the download itself is saying invalid or incomplete, just repeat the process to download again.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000