Cancel
Showing results for 
Search instead for 
Did you mean: 

64bit solid edge for students

N/A

was wondering how i can download the 64bit version of solid edge st4 for students? i can only find 32bit

2 REPLIES

Re: 64bit solid edge for students

Pioneer
Pioneer
The Student Edition is ONLY available in 32bit. It will run fine on a 64bit OS. We took the decision to make it as easy as possible for Students to obtain and use Solid Edge. The Solid Edge University Edition is available in both 32 and 64 bit and schools, colleges, and universitiy customers using the University Edition can make it available to their students.

Re: 64bit solid edge for students

Siemens Master Siemens Master
Siemens Master
As Doug says, you can run 32 bit on 64 bit OS. The only reason for a 64 bit SE is if you are doing assemblies of 50,000 parts or that kind of thing. Guessing you might graduate before you have time to model enough parts to choke 32 bit SE. :-)