Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: A Sneak Peek into Solid Edge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ditto on the variable table. As well as Rev Man. We'll see

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: A Sneak Peek into Solid Edge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I like the "tabbed" windows for all the open files, and the ability to put a single feature in multiple bodies!



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: A Sneak Peek into Solid Edge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Grundey wrote:

I like the "tabbed" windows for all the open files, and the ability to put a single feature in multiple bodies!


 

AMEN to the tabbed windows Ken.

 

My other user [ex: SaladWorks guy] loves to have lots of minimised files, and struggles with what file is what, rather than using "Switch Windows".

This "Tabbed" windows deal [assuming a preview "mouse-over" popup is going to be used] will help, both of us, manage our open documents at a glance.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: A Sneak Peek into Solid Edge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Does Martha Stewart do Salad Modeling?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: A Sneak Peek into Solid Edge ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bshand wrote:

Does Martha Stewart do Salad Modeling?


Hahaha.....clearly does Bruce,...but upon advise, she's not allowed to say. Robot wink

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: A Sneak Peek into Solid Edge ST9

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I have shared the Solid Edge ST 9 new features from my perspective and their application on my friend's website Daily-CAD-CAM.

 

Here's a quick list based on the SEU session:

1. Revision Manager 2.0
2. SolidWorks Drawing Migration
3. Customization and Preference Management
4. Support for High Resolution Monitors
5. A Tabbed Document UI
6. Sheetmetal Clash in Flat
7. Tolerance Table
8. Multi-Body Features
9. Solid Sweep
10. Spiral Curve
11. Teamcenter Tab on Command Ribbon
12. Assembly Relationship Manager
13. Variable Table Enhancements
14. New Drafting Features
15. Pack-n-Go

 

~Tushar Suradkar

www.CADVertex.com

 

Re: A Sneak Peek into Solid Edge ST9

Phenom
Phenom

I nag a lot on SE, but there is one thing I would like to say, SE is still the best solution for our 3D work and I like the speed of introducing new features!

 

If it's good, it's good. Smiley Wink

 

Thanks crew!

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user