Cancel
Showing results for 
Search instead for 
Did you mean: 

ADD 7/16-16 THREAD

Creator
Creator

 

 

  • Add hold dim.62in
  • Add 7/16-16 THREAD
  • BUT CHANGE THE DIM HOLD TO .438(7/16)

I DID NEED HOLD SIZE TO CHANGE WHEN ADD THREAD IN.

 SEE  Attachments

1 REPLY 1

Re: ADD 7/16-16 THREAD

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Ed2,

 

Looks to me like you need to use a counterbored hole....to have the 0.62" hole & the 7/16" threaded hole.

 

ST10_HoleOptions_Counterbore.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000