Ability to add a "group" of components to an assembly.

Phenom
Phenom

This is a follow up question to the abilty to "pack" the components in the Path Finder.

 

This question goes to the workflow of adding hardware stacks to an assembly.

 

I would like to pull a set/stack of components from a library and populate my assembly. Is there a way to define a group of components like a bolt+washer + another washer + nut and have this set come into the top assembly as individual components? Or an alternative would be to add the components as sub-assy and then move the components up into the main assembly? Upon adding this set could it automatically generate a group?

 

This would provide the user to quickly populate their design hardware.

 

2 REPLIES

There is Fastener Systems which requires the Standard Par...

Esteemed Contributor
Esteemed Contributor

There is Fastener Systems which requires the Standard Parts to be set up:

http://support.industrysoftware.automation.siemens.com/training/se/106/en_US/index.html#uid:fastener...

 

and there is the Systems Library function:

http://support.industrysoftware.automation.siemens.com/training/se/106/en_US/en_US//selfPacedExt/pdf...

 


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: There is Fastener Systems which requires the Standard Par...

Phenom
Phenom
Thanks Ken. I'll take a look at the documentation.