01-07-2015 04:21 AM
Hi,
I want to edit part in context in assembly for this part by click to part then use Edit In Place command, but it open the part I want to edit,,,Please try these files in attached. Any ideas.
Thanks,
Khang
Solved! Go to Solution.
01-07-2015 04:33 AM
This happens when the part you want to edit in place is already opened in solid edge; close it and the edit in place function will back to work.
01-07-2015 04:41 AM
02-24-2016 07:12 PM - edited 02-24-2016 07:16 PM
I'm having exactly the same issue, but do not have the part open (prior to editing in place - you can see this in the images as the Switch Windows button is grey'd out). I'm finding so many little issues like this since upgrading to ST8...! I have the latest Maintenance Pack installed (#5).
See images below:
02-24-2016 09:23 PM
This seems to be just the "Hide Previous Level" has been selected (maybe mistakenly using the shortcut Ctrl Q).
02-24-2016 09:29 PM - edited 02-25-2016 01:13 PM
Thanks very much for your prompt attention, really appreciate it. This has solved our issues. None of us were aware of this shortcut.
12-19-2016 04:24 AM
Thats excellent,
Solved our issues too, knew something had changed.
Thanks