Cancel
Showing results for 
Search instead for 
Did you mean: 

About changes in measures in the ISO draft file

Creator
Creator

Hello!

 

I drew some pieces in the ISO part file, and I made the assembly in the ISO assembly. Then, when I made a template in the ISO draft, I realized that some measures are wrong.

 

So, my question is, if it's possible to change some measures in the ISO draft file, and these changes are propagated to both ISO part and ISO assembly files?

 

Thanks!

4 REPLIES

Re: About changes in measures in the ISO draft file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
No - Solid Edge does not allow drafts to update the model.
One of the reasons is that you could easily destroy the integrity of the model or assembly with out realising that you had done so.
Whenever I see a CAD system with the ability to alter a model from the draft I shudder and think "toy CAD system" Smiley Happy

Cheers & seasons greetings
Mark

Re: About changes in measures in the ISO draft file

Creator
Creator
Thanks!

I'm a begginer on solid edge, so I'd like to know what's the best approach
to solve this issue?

Re: About changes in measures in the ISO draft file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Simply double click on the draft view you want to edit and Solid Edge will open the assembly or part which the draft view depicts.
If you are drafting an assembly then you can select the part you wish to edit.

Cheers
Mark


Sent from my iPad

Re: About changes in measures in the ISO draft file

Creator
Creator