Cancel
Showing results for 
Search instead for 
Did you mean: 

Add Binder to Pathfinder? Possible?

Pioneer
Pioneer

Is it possible to add the binder to the pathfinder? So anybody that opens up the components can open the bider straight from the pathfider.

 

Thanks for any help you may provide.

14 REPLIES

Re: Add Binder to Pathfinder? Possible?

not that i am aware but you should work with your VAR to submit an ER.

 

Re: Add Binder to Pathfinder? Possible?

Pioneer
Pioneer
Is there any way to add a note section or just a word file to the Pathfinder?

Re: Add Binder to Pathfinder? Possible?

Siemens Phenom Siemens Phenom
Siemens Phenom

@JustBillme wrote:
Is there any way to add a note section or just a word file to the Pathfinder?

 

No

Re: Add Binder to Pathfinder? Possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just a thought: Perhaps you could add a callout which would be in the PMI group in the pathfinder which you could rename to something meaningful for your purpose.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Add Binder to Pathfinder? Possible?

Pioneer
Pioneer
Good thought. I will see if I can make that work. Thank you.

Re: Add Binder to Pathfinder? Possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Let us know...

It does seem odd that you can't see that something is embedded via the binder unless you open the binder.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Add Binder to Pathfinder? Possible?

Pioneer
Pioneer

It kinda works and kinda not. You can add a note via the annotation. But then its just this big note hanging out in mid air and only visible in 2 planes. I guess it can serve a purpose but it sure is clunky and not very nice looking.

Re: Add Binder to Pathfinder? Possible?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

At least you can turn it off and on at will.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Add Binder to Pathfinder? Possible?

Pioneer
Pioneer
There is that LOL. Thank you for the suggestions.